我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How can legacy PWX , Concept or PL7 projects be converted to M580?
There are no means for taking the Legacy project straight to M580. There are no planned changes in this area.
  1. Conversion from Legacy to Unity Quantum/Premium is done with the embedded converter in Unity Pro
  2. Conversion from Unity Quantum/Premium to M580 is done with the Unity M580 Application Converter.
  3. If moving forward, it is necessary to convert from M580 w/QNTM IO to M580 with X80 IO that can also be done with UMAC.