我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How can you set the timeout settings on the ATV71 drive using IO scanner and Ethernet TCP-IP?
Issue:
Setting the timeout on the ATV71 drive using IO scanner and Ethernet TCP-IP

Product Line:
ATV71

Environment:
All

Cause:
Loss of communications from the Ethernet.

Resolution:

If the customer needs to change the time out for Ethernet communications he can do it from the web page  or the (Tout) parameter in the drive.

The default is 2 seconds.

See the attachment.

施耐德電機Taiwan

附件
Ethernet timeout settings on webpage.jpg [115.12 KB]