我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
B10d calculation for normally closed contact ZBE102 ?
FOR NORMALLY CLOSED CONTACT (ZBE102)
The fault exclusion described in Table D8 from ISO 13849-2 2012 can be considered
As our contact ZBE102 respects requirements and verification test according to the IEC 60947-5-1:2003 Annex K “Special requirements for control switches with direct opening action”, so the B10d cannot have to be considered thanks to the exclusion fault.

施耐德電機Taiwan

附件
17-017 C&S B10d for ZBE102.pdf [218.36 KB]
ISO 13849-2 2012 Table D8.docx [150.26 KB]
探索更多
產品:
探索更多
產品: