我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is it possible to use Modbus port for Modbus RTU communication and Graphical panel VW3A1111 for ATV320 drives?
On ATV320, VW3A1111 (or any display via modbus serial) and modus RTU communication cannot be used at the same time.