我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What can cause an INF4 fault on the ATV32 Drive?
Issue:
INF4 fault on the ATV32 Drive

Product Line:
Altivar ATV32 drive

Environment:
All

Cause:
Flash memory or EEPROM Issue

Resolution:
Try removing any option cards on the drive first and then Power cycle. If the fault does not clear then there may be an internal issue on the drive and it will need to be replaced.