我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is there certification and accreditation for PM5110?
Product Line
PM5110

Environment
Certification

Resolution
The PM5110 meter has SGS certification from the external lab.

Refer the attached type test report of PM5110 and  accreditation of SGS lab.

施耐德電機Taiwan

附件
SGS UK - UKAS accreditation.pdf [502.74 KB]