我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What's the basic or typical combination of XVU range?
The basic or typical combination of XVU range as below:
Without Buzzer: Base unit (XVUZ0x) + AC body or DC body (XVUC21x) + LED lights (XVUC23~XVUC29)
With Buzzer: Base unit (XVUZ0x) + AC body or DC body (XVUC21x) + LED lights (XVUC23~XVUC29) + XVUC9S(x)
With Sound: Base unit (XVUZ0x) + AC body or DC body (XVUC21x) + Sound unit (XVUC9V) + LED lights (XVUC23~XVUC29)
With PWM units: Base unit (XVUZ0x) + AC body or DC body (XVUC21x) + XVUC9VP and / or XVUC29VP