我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
ATV680- Do the input wires and motor wires come in the top or bottom?

Issue:
Do the input wires come from the top or from the bottom on ATV680

Product Line:
ATV680

Resolution:
According to the ATV680 Handbook (NHA37113) , the input power wiring and motor wiring come from the bottom of the enclosure.   To wire from the top, they will need a Q  option ( Door Mounted Overload Reset Push Button) & U option (Top Entry Cubical )

See page 95 of The ATV680 Handbook.

施耐德電機Taiwan

附件
ATV680_Handbook_EN_NHA37113_02.pdf [7.46 MB]