我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can the PMESWT0100 be used in M580 HSBY configuration?
Goals and Symptoms

Can the PMESWT0100 weighing module be used in M580 HSBY configuration?


Facts and Changes

Unity pro, M580, PMESWT0100


Causes and Fixes

The use of PMESWT0100 module in M580 RIO in the case of HSBY configuration has not being tested and validated hence should be avoid.