我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can Altivar Process variable speed drive ATV900, ATV600 withstand environment with chlorine?

One of the environmental condition in Altivar ATV650 datasheet deals with chemical pollution resistance.
For ATV reference it is possible to find
Chemical pollution resistance : class 3C3 EN/IEC 60721-3-3

The standard defines the levels of chemical active substances. For 3C3 class, max concentration of chlorine can achieve 0.3mg/m3 (average) or 1mg/m3 peak value.
Average value is expected long-term value. Peak value can occur over a period of time of not more than 30 minutes per day.