我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is the PDU removable that's included inside the NetShelter CX AR4000MV?
Issue:
A customer wants to replace the PDU in a NetShelter CX Mini.

Product Line:
NetShelter CX

Environment:
AR4000MV, all serial numbers.

Cause:
The brochure doesn't show if the PDU is removable.

Resolution:

The PDU that ships installed inside the AR4000MV is removable.