我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to configure the BMXNOM200 for 'Stop on Reception' using both CR and LF
Issue
How to configure the BMXNOM200 for 'Stop on Reception' using both CR and LF

Product Line
BMXNOM0200

Environment
Unity, Windows 10


Resolution
To configure the NOM serial port for the Stop on recption using both CR and LF, reference the example in the following screen capture.

ffff