我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What terminal blocks can be used with a BMXDRA0805 I/O module?
BMXDRA0805 I/O module can be used with one of the following terminal blocks:

- BMXFTB2000 - Cage clamp
- BMXFTB2010 - Screw clamp
- BMXFTB2020 - Spring clamp

The terminal blocks will have to be ordered separately, the BMXDRA0805 I/O module does not come with any terminal block.