我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to check the warning messages, using SoMove for Altivar Process Drive ATV630 and ATV930?
Issue:
Checking the warning messages using SoMove for the ATV630 and ATV930 drives.

Product Line:
ATV630, ATV930

Environment:
All serial numbers

Cause:
NA

Resolution:
In SoMove software, click on "Diagnostics" and it will display the "Active Warning", "Warning History", and "Warning Groups" under Drive Menu on the left side window.  Select the warning menu that you want to check.