我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the IP degree of protection of the new Harmony + products ?
The global range is IP66, IP67, IP69 and IP69K, find a declaration of conformity where you can find the sub-families which are concerned.

施耐德電機Taiwan

附件
18-006 C&S Harmony d22mm heads IP66, IP67, IP69, IP69K.pdf [44.72 KB]