我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How does one program the ATV212 Drive so that RY relay will trigger when a speed threshold is reached?
Issue:
ATV212 configuration so that RY relay will trigger when a speed threshold is reached

Product Line:
Altivar 212

Environment:
All

Cause:
Frequency reference reached

Resolution:
Using RY relay for speed reached functionality.
F130 from the factory is already programmed as 4 for speed reached.
F100 can be programmed to value desired in hz.

The RY relay will actuate when the VFD output frequency is greater than or equal to the F100 setting.

施耐德電機Taiwan

探索更多
產品:
探索更多
產品: