我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Program Viewer web page for the BMENOC0311 returns the error 'Couldn't dynamic plc content'.
Issue
The Program Viewer web page for the BMENOC0311 Factorycast module returns the error 'Couldn't dynamic plc content'.

Product Line
BMENOC0311

Environment
Windows 10


Resolution
The Program Viewer web page for a BMENOC0311 Factorycast module returns the error 'Couldn't dynamic load plc content.
nbg





This will occur if the Unity application project settings is not configured for the  Program Viewer.

To resolve the issue:
  • Open the Project Settings for the Unity application.
  • Click on 'PLC Diagnostics'
  • Select the checkbox labeled 'Program Viewer Information'
  • Click on 'Apply'.
  • Click on 'OK'.
dgd