我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How many BMXEIA0100 (AS-interface module) can be configured in a M580 architecture?
Issue

How many BMXEIA0100 can be used in a M580 architecture?

Product Line

M580, BMXEIA0100

Resolution

16 is the max number of BMXEIA0100 AS-i modules accepted in M580 configuration. This is the global limitation for the M580 system.
With have other limitations on drops & local CPU rack:
=> 2 max on RIO drops with CRA
=> 2 max on level 10 CPU, 4 max on level 20, 6 on level 30 and 8 for above.