我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is a BMEAHI/BMEAHO card only configurable with DHCP in a M580 architecture?
Issue

Is a BMEAHI0821 card only configurable with DHCP in a M580 architecture?

Product Line

BMXEAHI0821

Resolution

The FDR (faulty device replacement) functionality is a feature used by CPU/NOC to assign the same IP and configuration to a new BMEAHI0821 module when replacing a faulty one on the same rack/slot. The module gets its IP only via DHCP (dynamic host configuration protocol) and configuration is transferred from the FDR server of the CPU or NOC.