我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Which types and sizes of wires can be connected to the PRA90047 terminal?
In the PRA90047 it is possible to mount the following wires:
- from 0.5mm2 to 4mm2 - solid, flexible or flexible with ferrule.
- from 0.5mm2 to 6mm2 - solid or flexible (without ferrule).