我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Which drives offer thermal monitoring of the braking resistor?
Issue:
Drive selection for thermal monitoring of the braking resistor.

Product Line:
Altivar drives

Environment:
ATV340, ATV930

Cause:
Braking resistor thermal monitoring

Resolution:
Both the ATV340 and ATV930 offer braking resistor monitoring including thermal state.