我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Why is the Local/Remote selection not showing up under the R1 selection table in the IO relay configuration?
Issue:
The Local/Remote configuration on IO Relay.

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
They want the R1 relay to show Local or Remote status

Resolution:
Check your firmware version it needs to be version V1.6IEXX or above for this feature to be available.