我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the Unity Pro version compatible with the PRM Gateway DTM v1.3.0.0?
Issue
This resolution clarifies the minimum version of Unity Pro compatible with the PRM Gateway DTM v1.3.0.0.

Product Line
EcoStruxure Control Expert, M580, PRM (TCSEGPA23F14F)

Environment
Unity Pro v11.1, BMEP581020 v2.50, PRM

Resolution
The PRM gateway DTM v1.3.0.0 is compatible with Unity Pro v11.1 or later.