我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Do we offer a NEMA 3R flange kit on the ATV600 and ATV900 process drives?
Issue:
Are the NSYPTDS5 Flange kits NEMA 3R rated?

Product Line:
NSYPTDS5

Environment:
All

Cause:

Resolution:
Flange kit  NSYPTDS5 + ATV630/ATV930 drive association has not been approved to be NEMA but has qualified to be IP55 only conforming too IEC standards.