我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
A-RUN_PRIM / B - RUN STBY / TASK OVERUN is Displayed in Status Bar while Connected to M580 HSBY CPU 6040 Unity 13 XLS However %S19 is set to Zero
When FAST task is created and there is no section in FAST task, then TASK OVERRUN is displayed

you can either Delete FAST task if it's not used. or at least create  one section with very simple logic to avoid this error