我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the ATV320 24Vdc logic input loading?
Issue:
What is the consumption on the ATV320 digital inputs?

Product Line:
ATV320

Environment:
All model numbers, all serial numbers

Cause:
Calculating external power supply requirements

Resolution:
The ATV320 digital inputs, DI1 thru DI6, consume 7mA each.  The STO input consumes 16mA.