我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Video: Where can I check the Input Output Map on the ATV320 drive?
Issue:
Checking Status of Digital Inputs on ATV320 drives

Product line:
Altivar 320, ATV320

Environment:
All models in range

Cause:
Troubleshooting and testing

Resolution:
The ATV320 has the ability to check the status of the Logic or Digital inputs.

On the default display navigate to NON > ION > LIA > LISI.
On this screen you will see the logic input state and be able to determine if the inputs are opening and closing as needed.

施耐德電機Taiwan

附件
ATV320 LISI.JPG.jpg [41.69 KB]