我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to install and connect an IFE module and TRV00210 units [Video]
Resolution:
Install IFE module on din mount. Ensure that the back connector lines up with that of the connect on the din rail.
Install TRV00210 units similar to that of the IFE module, ensuring that the connectors are all aligned.
Supply power to the din rail. To verify correct installation, the units’ LEDs will indicate and flash.

The objective of this video is to provide guidance for installing an IFE module with TRV00210 units on a din mount