我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the replacement HOA Selector switch for the ATV660 enclosed drives?
Issue:
Need a replacement Hand Off Auto Selector switch for the ATV660 enclosed

Product line:
Alticar 660, ATV660

Environment:
Standard enclosed products.  Check the description on the order for confirmation that the drive does not list special operators.

Cause:
Replacement or spare parts

Resolution:
Standard 3 position operator is ZB5AD3
Standard mounting collar is ZB5AZ009
Two contact blocks, each is ZBE205
Standard legend plate is 65170-166-17
Legend plate holder is ZBZ32