我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Does the ATV320 drive have pump control parameters?
Issue:
Are there pump control parameters in the ATV320 drive?

Product Line:
ATV320 drives

Environment:
Pump Control parameters

Cause:
n/a

Resolution:
The ATV320 has PID parameters, but not pump control.  For Pump Control parameters, would suggest the ATV630 drive.