我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
ATV320 drives do they come with integrated Bluetooth communications?
Issue:
Bluetooth availability on the ATV320.

Product Line:
ATV320

Environment:
All

Cause:
Bluetooth

Resolution:
The ATV320 drives both Versions C and B do not have a built-in Bluetooth option.