我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What functions can be assigned to an ATV212 logic input?
Issue:
Trying to assign functions to an ATV212 logic input.

Product Line:
ATV212

Environment:
All models

Cause:
Explore VFD control options

Resolution:
The ATV212 has assignable logic input terminals F / R / RES / VIA.
Please see the attached file for all Logic Input Functions

施耐德電機Taiwan

附件
ATV212 Logic Input Functions.pdf [1.93 MB]