我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the part number for an ATV320 encoder option card?
Issue:
ATV320 encoder option card part number.

Product Line:
Altivar 320

Environment:
All

Cause:
Part number needed

Resolution:
The encoder option card part number is VW3A3620.
https://www.se.com/ww/en/product/VW3A3620/speed-monitoring-module---rs422---5v/