我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to connect motor encoder to Lexium LXM32 drive if the motor has been previously connected to LXM05 drive?

LXM05 used Molex connector for connecting the encoder.
LXM32 uses RJ45 connector so the best is to use encoder adapter cable VW3M8111R10.

施耐德電機Taiwan

附件
VW3M8111R10.jpg [30.65 KB]