我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Video Altivar Process: How to connect to webserver?

Article available in these languages: 荷蘭文

Altivar Process ATV600 or ATV900 have a Webserver embedded !
How to connect your computer to the Altivar to see the Webserver page on your browser ?
(Ethernet, WIFI, Bluetooth, IPV4,6 Modbus, PROFINET ….)

Description also to connect to Wifi with the WIFER option (TCSEGWB13FA0).



Related video: "Altivar Process: What are the Webserver's main features?"