我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to display several panels of a Vijeo Designer application using in same time several targets and HMIZMDARX Multi Display Adaptor?
Goal:  To display two different panels of a same Vijeo Designer project with panel 1 displayed on the Host HMIG5U2 and panel 2 displayed on the Client through the Webgate.
To test, we’ll use:
- a HMIG5U2 with HMIDT551 as Host and
- a HMIDT551 with HMIZMDARX module as Client.

Please refer to the attached pdf document.

施耐德電機Taiwan

附件
FAQ_Multi display projet.pdf [2.82 MB]