我们今天能为您提供什么帮助?

NetBotz 700 | Where can I get the SNMP MIB for the NetBotz 750?

Issue:
Where can I get the SNMP MIB for the NetBotz 750

Product Line
NetBotz 700 Series

- NetBotz Rack Monitor 750 (NBRK0750)


Environment:
NetBotz 750 SNMP MIB

Cause:
With the release of the gen-5 NetBotz 750 units, a new SNMP MIB must be used

Resolution:

You can obtain the NetBotz version 5 MIB at the following location:
https://download.schneider-electric.com/files?p_enDocType=Firmware&p_File_Name=netbotz50.mib&p_Doc_Ref=APC_SFNB5_MIB

Please note that with newer firmware, the MIB file can be downloaded directly from the device.