我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to execute Autotuning for Altivar ATV frequency inverter drives remotely via its DTM in PLC or ePAC Modbus controllers like?
When a drive DTM is added in Unity DTM browser and the drive is connected to PLC over ethernet (Modbus TCP or Eth IP), then the autotuning can be executed from the vertical menu.
Parameter TUN (to execute autotuning) is not available in ATV DTM configuration.
Attached picture shows the menu to access autotuning. Right-click on Device in DTM browser, select Device menu-Additional functions-Autotune.

施耐德電機Taiwan

附件
Autotuning via Unity_DTM_online.jpg [473.59 KB]