我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Which encoder card for Altivar ATV71 Frequency inverter drives are compatible with sincos encoder?
The only encoder card for ATV71 compatible with sincos encoder is VW3A3409.
Nevertheless, this encoder card cannot be placed in standard ATV71 drive. You have to use ATV71...S383 version (version that could control asynchronous or synchronous motors).
ATV71...S383 is not commercialized, unfortunately, therefore it makes sense to upgrade original assembly to ATV930+ analog encoder card.
FYI, attached is the catalog with encoder cards for ATV71.

施耐德電機Taiwan

附件
altivar71optionsencoderinterfacecards_characteristicsreferencespresentation_en4.1_60285.pdf [73.06 KB]