我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
ATV660: Using the VW3A3203 for a Thermal Sensor

Article available in these languages: 西班牙文

Issue:
Set up AI4 for a Thermal Sensor using VW3A3203.

Product Line:
ATV660

Environment:
Thermal Sensor

Cause:
n/a

Resolution:
Response from France:
VW3A3203 card accepts standard Pt100 sensors for the range -20…+200 C deg
The temperature value is given at: TH4V (AI4 thermal value, @13252, unit: 0.1Cdeg )
The following settings are necessary:
AI4T = Pt100 in 3 wires (AI4 type)
TH4S = Yes (Activation of the thermal monitoring on AI4. )
You do not need to adjust any other parameters.