我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the polarity of A and B Terminals when using BACnet on ATV212 drive?
Issue:
Polarity of A and B Terminals when using ATV212 BACnet.

Product Line:
ATV212, Altivar 212

Environment:
All

Cause:
NA

Resolution:
Terminal B is positive(+) and terminal A is negative(-).