我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How can the Altistart ATS48 soft starter be wired up for the 2 wire run control to start the motor?

Issue:
2 Wire Control on ATS48

Product Line:
Altistart ATS48

Environment:
All

Cause:
Basic two-wire control

Resolution:
Wire the soft starters supplied +24vdc through your dry maintained contact back to the soft starters run and stop jumpered terminals.

See the ATS48 user manual for the terminal block connections.
https://www.se.com/us/en/download/document/1494409/


施耐德電機Taiwan

探索更多
產品:
探索更多
產品: