我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What can cause a Backlash error [bS9F] fault on an ATV340 series drive?
Issue:
Customer is experiencing a bS9F Backlash error on an ATV340 series drive.

Product Line:
ATV340

Environment:
Backlash Compensation function is being used.

Cause:
The torque threshold used for backlash function can not be reached after [BL Monit Delay] bqt.

Resolution:
 Verify the settings
 Verify the coupling