我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can I assign a second Run forward command to Altivar Process drives?
Issue:
Assign a second Run Forward command to Altivar Process Drives Logic input.

Product Line:
Altivar Drives, ATV600, ATV900

Environment:
All

Cause:
Want to install a separate remote external +24vdc start/stop command to DI3

Resolution:
No, You can not assign 2 "Run Forward" commands to different logic/digital inputs.