我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is there a way in Ecostruxure Control Expert/Unity Pro SFC to go to a specific Step?
Issue:
Equivalent function to RSLogix5000 SRF instruction.  When this instruction is true, it forces the SFC to go to a specific step defined by the instruction.

Product Line:
Momentum
M340
M580

Environment:
Ecostruxure Control Expert/Unity Pro ​

Resolution:
The equivalent in function block in Ecostruxure Control Expert is the SETSTEP.  This FB is part is the System and SFC management library.