我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is a competitive cross for Cutler Hammer 92-01943-01?
Issue:
Looking for a replacement HMI with a physical keyboard to replace a Cutler Hammer 92-01943-01.

Product Line:
Magelis HMIGK

Resolution:
The competitive cross for the Cutler Hammer 92-01943-01 is the HMIGK2310. The HMIGK is programmed with Vijeo Designer V6.2 SP5.1 or higher.