我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
On the PowerTag A9 F63 model, ref. A9MEM1562 if I try to be consistent with the flat cable position, the LED of the module is upwards. Should I twist the flat cable to have the LED down?
This has no impact on the operation but to be consistent with the rest of the range we favor the Led down, and in this case, the flat cable is twisted.