我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How does Altistart ATS480 measure the torque?

The ATS480 calculates the motor torque based on the current, because when a motor has constant voltage and frequency, the amount of torque is directly proportional to the amount of current.
Rated torque is not defined in Altistart, so the torque value is only relative (referred to rated torque Tn)
This value of relative motor torque is used in function like motor underload monitoring (ULL), threshold set in LUL (underload threshold)