我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Why might I get an NST on my ATV320 when I wire a relay to the digital output (DQ)?
Issue:
Getting NST on my ATV320 when wiring a relay to the digital output (DQ).

Product Line:
Altivar 320

Environment:
All

Cause:
NST on the ATV320 with relay connected

Resolution:
1. Check to make sure your relay is wired correctly in series with the digital output:
Jumper +24V to DQ+
Wire your + side of your relay coil to DQ-
Wire the other side of the coil to COM
2. Measure the amperage pull of your relay. The digital output and the drive's +24V supply each have a maximum 100mA capacity.
If your relay is pulling more than 100mA, it's pulling down the +24V in the drive and causing the NST.
See attachment.

施耐德電機Taiwan

附件
FAQ 86814.png [25.69 KB]