我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Altivar 320 Variable Speed Drive: Programming a Flashing Output Signal Using Logic Functions

Article available in these languages: Czech

Using 2 timers it is possible to program a flashing signal.
Min setting is 0.1second up a level, 0.1second down a level.
See Altivar 320 logic in the attachment.
The output of the logic is connected to relay output (for test only)
The first timer defines period of the signal, second timer defines duration of the signal up a level

施耐德電機Taiwan

附件
Flashing signal.jpg [42.73 KB]
ATV_flashing_signal.zip [2.12 KB]